Add Custom Notes

This option is available only when the Quick Capture mode is enabled.

Add custom notes to be saved along with your screen capture. Notes will be saved as an ASCII text file (.TXT file extension) with the same file name as the screen capture. No formatting of the text is available.

By default, the notes are saved each time a new screen capture occurs. To clear your notes after each screen capture, select the "Clear After Image Saved" box in the Capture Settings drop-down panel.

Chart Right-Click Operations

Right-click anywhere on the Notes field to display these options:

Cut - Cut (delete) the highlighted text from the Notes field. To select all of the text contained in this field, use the keyboard shortcut Ctrl+A.

Copy - Copy the highlighted text from the Notes field to the Windows Clipboard. To select all of the text contained in this field, use the keyboard shortcut Ctrl+A.

Paste - Paste the contents of the Windows clipboard into the Notes field.